The premier cooling tower maintenance, parts, and service plan in North America.
EXTEND ADVANTAGE is for high-demand operations that require the most comprehensive levels of service from industry technicians. With top-tier services and fixed annual prices, ADVANTAGE ensures your cooling towers are working at their optimum levels so your systems can too.
EXTEND ALLIANCE is for when you need a maintenance and repair team on-site but don’t want the additional expense. Providing a local presence to meet your site’s specific requirements, ALLIANCE gives you access to SPX’s cooling tower experience right when you need it — minimizing costs as well as response times.
EXTEND ASSURANCE provides your operation with preventive maintenance at an affordable price.
For additional program details, please contact your SPX Cooling Technologies representative or call
1-800-4MARLEY.
Consistency is one of the keys to success for most manufacturing companies. Plant managers want to make consistent high quality products, maintain consistent costs, and have consistent day-to-day operations at their site.
The customer in this case is a global company that produces plastic resins for use in packaging applications. Such complex manufacturing operations generate a lot of heat and other complications. Any small deviation from standard process conditions could generate hours of inferior product quality.
After years of occasional failures due to insufficient maintenance and the resulting unpredictable maintenance costs, the customer considered implementing a regular preventive maintenance program for its cooling towers. It trusted SPX Cooling Technologies to perform the cost-benefit analysis of such a program.
However, before any such program could be implemented, the customer suffered a disastrous, quarter million dollar failure of four cooling tower cells as a result of poor maintenance.
Consequentially, the plant decided that the SPX service program would be a perfect fit to prevent such failures in the future. For a fixed fee, the customer receives frequent pre-planned maintenance that includes thorough inspections of each cell at the plant and SPX replaces specific mechanical components upon failure, significantly reducing unexpected costs at the facility.
The greatest value that the customer has received is peace of mind. Today, whenever they encounter a cooling tower challenge they cannot manage themselves, they simply call SPX Cooling Technologies, knowing that the problem will be resolved by a leader in cooling tower technology.
Despite the critical role that cooling towers play in maintaining steady-state operation, large petrochemical customers sometimes have more important priorities than maximizing cooling tower performance.
Such companies could have anywhere from 10 to 100 or more cooling towers on site that dissipate heat from plant processes. Proper care and maintenance is required, and without dedicated crews to sustain peak performance, plant utilization could suffer.
One particular SPX customer historically used an in-house maintenance crew for upkeep of its on-site equipment and systems. However, as it became increasingly difficult for them to keep the cooling towers in peak operating condition, they sought a more efficient method of maintaining their cooling towers.
Having been a long-time customer, with the majority of its cooling towers being Marley towers, SPX Cooling Technologies took over cooling tower operations at the customer’s plant. In providing on-site coverage, SPX made preventive maintenance a priority, implementing proactive processes to maintain optimal performance.
Because of SPX, the customer now has the opportunity to concentrate its attention and resources on other important matters that affect product quality and smooth operation of the plant.
Peak-load power plants are critical to a utility’s ability to supply steady-state electricity to the power grid.
When an increase in power production is required, it is critical that the cooling towers are ready to serve the needs of the plant on quick notice.
One particular SPX customer operated a 600 MW coal-fired power plant with three cooling towers. Unfortunately, one of the site’s cooling towers was an older unit in poor condition as well as being an inappropriate design for the plant's increased cooling needs.
The aging unit was replaced with a Marley F600 fiberglass cooling tower.
To protect its new investment, the customer collaborated with SPX to develop a customized service plan that would maximize the performance of the tower.
A team of skilled Marley personnel now visits the new tower and performs general preventive and mechanical maintenance work on a pre-scheduled basis.
With SPX coverage, all 12 cells of the new tower are in peak condition, and since the start of the service plan, there have been no major issues that have hampered the performance of the cooling tower.
An added benefit of the EXTEND service plan has been giving the customer the peace of mind they need to focus on more pressing matters.